AnsweredAssumed Answered

RAppID BL Tools for S32K144

Question asked by 燕琳 赵 on May 13, 2019
Latest reply on May 20, 2019 by Jiri Kral

Dear expert

My development is based on S32K144 EVB –Q100. Now I meet a question on RAppID Boot Loader Utility. The version of RAppID BL tools is shown as following:

My steps are following:

1. insert openSDA USB prot, and there is a mass storage is shown on my computer:

2.I copy SK144_Bootloader.rbf into F disc:

3.the pins are configured as following:

Jumper

Configuration

Description

J104

1-2

Reset signal to OpenSDA,used to enter into OpenSDA Bootloader mode

J107

1-2

S32K144 powered by 12V power source.

4.only push the “reset” button on EVB, not power off.

5.open the “RAppID Boot Loader Utility”,and setings are shown as following:

6.but the error is shown as following:

7.I have tried some different rbf file, but the error is always the same. These rbf files are attached.

 Could you help me? my questions are:

1. Is the step 4 right? Should I power off the EVB after copy rbf file into mass storage device?

2.Need I copy *.rbm or rba file into the mass storage device?

3. how can I get the correct rbf file?

Thank you very much for your kind help!

Outcomes