iMX8M Mini in the sleep mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M Mini in the sleep mode.

955 Views
borisberman
Contributor III

Hello,

I would like to know if, besides the i.MX 8 M Mini LPDDR4  EVK,  the NXP has a special EVK or design for iMX8M Mini in the sleep mode.

I mean EVK /design which allows you to get the minimum power consumption, after the following command: 

"echo mem > /sys/power/state"

Thank You 

Boris

0 Kudos
1 Reply

684 Views
igorpadykov
NXP Employee
NXP Employee

Hi Boris

NXP provides only i.MX 8M Mini EVK design boards

8MMINILPD4-EVK Product Information|NXP 
8MMINID4-EVK Product Information|NXP 

There is also validation (arm2) board, it is internal board not intended for customer usage.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos