Dear Sir,
I wonder that if sabresd_6dq support 802.11w (pmf), I tried modfied driver to add pmf feature and set right option in wpa_supplicant.conf while using the wpa_supplicant which complied with 11W function but no work,is there something i have to modify?
B.R jerry
Hi Hung
yes BCM4339 used in BSPs as stated in Linux L4.14.98_2.0.0 Documentation
supports IEEE 802.11w — Secure Management Frame according to its datasheet
One can post question on murata support portal how to enable it
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------