AnsweredAssumed Answered

ADC Channels in LPC54608J512BD208

Question asked by Prasanna Naik on May 12, 2019
Latest reply on May 13, 2019 by xiangjun.rong

Hi ,   

 1)  I want to use all 12 ADC channels of LPC54608J512BD208 but PIO0_10/ADC0_0,PIO0_11/ADC0_1 and PIO0_12/ADC0_2 are shared with SWD interface pins SWO, SWCLK and SWDIO respectively.

   From datasheet i could see JTAG interface as well in this device. Can i use JTAG debug interface to debug this device as jtag pins are not multiplexed with any of the ADC lines. 

 

2) I have OM13092(Revision D) development board for evaluation of LPC54608 microcontroller. Can i test the above point on this development board.

 

jeremyzhousoledad Erich Styger

 

Thanks and best regards,

Prasanna

Outcomes