We use CPU is i.MX 6Quad_MCIMX6Q6AVT10AD,When we do the high temperature 75 ℃, USB video will be caton, the picture is not smooth, like lost frames!What could be the reason? How do I find out why?
We use CPU is i.MX 6Quad_MCIMX6Q6AVT10AD,When we do the high temperature 75 ℃, USB video will be caton, the picture is not smooth, like lost frames!What could be the reason? How do I find out why?
Thanks for your replay!When I test, I found that high temperature caton, CPU temperature is 92 ℃, the CPU frequency down to 400M, where is the temperature setting?What is the default software of high temperature?
Hello,
Your system is based on Linux 4.1.15 kernel.
Customers can use section 2.7 (Thermal) of i.MX_Linux_Reference_Manual.pdf
https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS
Regards,
Yuri.
Hello,
General thermal considerations (relations between ambient and junction temperatures)
are provided in app note AN4579 (i.MX 6 Series Thermal Management Guidelines).
In particular, customers can use thermal characteristics from i.MX6 Datasheet :
Tj = Ta + RthJA * Pd
Tj - junction temperature;
Ta - ambient temperature;
RthJA - Thermal resistance Junction to Ambient;
Pd - power consumption.
http://www.nxp.com/assets/documents/data/en/application-notes/AN4579.pdf
The mentioned "the high temperature 75 ℃", looks like, is ambient temperature, meaning
that the junction one may exceed the allowed maximum. This means i.MX6 normal operation
cannot be guaranteed. Perhaps a heat sink is need for the i.MX6.
Regards,
Yuri.