drag_and_drop flash failing on i.MX RT 1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

drag_and_drop flash failing on i.MX RT 1050

Jump to solution
1,152 Views
lucky1408
Contributor II

Hello,

I'm trying to flash my code on the IMXRT1050-EVKB, but every time I get a fail: "The transfer timed out."

The examples provided by NXP work perfectly, but when I try to flash my code I get a fail.

I'm using the drag-and-drop method.

I copied all the settings from the example into my settings, but that didn't help.

Is there something which needs to be done in order to make this work?

Or can it be that the bin file is to big? It's around 89 KB and the examples which I've tried are around 20 - 25 KB

IDE: IAR embedded workbench 8.30.1

With kind regards,

Luc

Labels (1)
0 Kudos
1 Solution
1,027 Views
lucky1408
Contributor II

Fixed it by changing the CMSIS DAP reset to "core" instead of "System"

With kind regards,

Luc

View solution in original post

0 Kudos
3 Replies
1,027 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Luc Aarts,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1) Is there something which needs to be done in order to make this work?
--  4.1. OpenSDA Drag/Drop and boot from QSPI Flash section in the application note: AN12108 illustrates the complete steps, please follow them.
Q2)  Can it be that the bin file is too big?
-- No, I don't think so.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,027 Views
lucky1408
Contributor II

Hello jeremyzhou,

I've followed the steps in that file and also the ones in AN12183, but I keep getting the following error:

"Verification error at 0x60000000: mem = 0x00, file = 0x46"

Do you know what this means?

With kind regards,

Luc

0 Kudos
1,028 Views
lucky1408
Contributor II

Fixed it by changing the CMSIS DAP reset to "core" instead of "System"

With kind regards,

Luc

0 Kudos