I want to drive a 8x24 LCD drive. LCD voltage is 3V and f = 51 Hz. via MC09S08LL16 microcontrller.
Problem; When I set more than 3 segment on the same Frontplane the other segments are also appear but they are weak.
If I set only one segment this segment is also weak. 1 to 3 segment is working fine. The position of the segment doesnt care, but they must be on the same FP.