Hi
I'm follow the Auto_Linux_BSP_20.0_User_Manual.pdf
and i'm done 2.1.1 Building default YOCTO except " repo init -u ssh://git@bitbucket.sw.nxp.com/alb/auto_yocto_bsp.git -b develop -m default-bitbucket.xml " and "bitbake <imagename>"
It's written on the manual that "If the machine chosen was s32v234evb, after the successful finalization of the build, the results will be placed in the build_s32v234evb/tmp/deploy/images/s32v234evb directory. Results for other machines will be placed in similar directories, but named according to the machine name.
This release includes support for:
• Machines: s32g275sim, s32v234bbmini, s32v234evb28899, s32v234evb, s32v234pcie, s32v234tmdp, s32v344sim, s32r45xsim, s32v234evbubuntu, s32v234sbc, s32v234ccpb
• Images: fsl-image-base, fsl-image-auto, fsl-image-ubuntu, fsl-image-ubuntu-base"
but I can't find directory 'build_s32v234evb/tmp/deploy/images/s32v234evb' ( i use s32v234evb ) and images like fsl-image-base too.
I think the cause is " repo init -u ssh://git@bitbucket.sw.nxp.com/alb/auto_yocto_bsp.git -b develop -m default-bitbucket.xml "
but when i typed the "repo init -u~" in the terminal
it respond
"ssh: connect to host bitbucket.sw.nxp.com port 22: connection refused
fatal: could not read from remote repository.
Please make sure you have the correct access rights
and the repository exists.
fata: connot obtain manifest ssh://git@bitbucket.sw.nxp.com/alb/auto_yocto_bsp.git"
I think bitbucket.sw.nxp.com server is down..
Anyway
how to get the auto_yocto_bsp.git? and where is the Images like fsl-image-base
bitbucket.sw.nxp.com is working?
Thanks