uuu 无法自动解L4.9.123_2.3.0-ga_images_mx8mm.zip压烧录固件

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uuu 无法自动解L4.9.123_2.3.0-ga_images_mx8mm.zip压烧录固件

3,151 Views
1223656192
Contributor I

uuu 工具在win7 下无法自动解压烧录L4.9.123_2.3.0-ga_images_mx8mm.zip。 UUU log如下:

D:\Train\NXP\tools\uuu>uuu L4.9.123_2.3.0-ga_images_mx8mm.zip
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.91-0-g3799f4d

Your console don't support VT mode, fail back to verbose mode
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
Wait for Known USB Device Appear...

Error: fail open file: >L4.9.123_2.3.0-ga_images_mx8mm.zip/fsl-image-validation-imx-imx8mmevk.sdcard [?25h

另外执行 uuu  fsl-image-validation-imx-imx8mmevk.sdcard.bz2,同样无法打开.sdcard.bz2压缩,(Error: fail open file:

Labels (1)
0 Kudos
4 Replies

2,482 Views
1223656192
Contributor I

你好,和L4.9.123_2.3.0-ga_images_mx8mm.zip 里面uuu.auto脚本文件的FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard 这句有关系。L4.9.123_2.3.0-ga_images_mx8mm.zip 里面没有.sdcard后缀的文件,只有fsl-image-validation-imx-imx8mmevk.sdcard.bz2  但除了手动解压出.sdcard再执行烧录,还有什么别的方法么?

0 Kudos

2,482 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

In the windows 7 you need to install driver, you also can see uuu usehttps://community.nxp.com/docs/DOC-342719 here for windows 10 and windows 7.

0 Kudos

2,482 Views
1223656192
Contributor I

你好,文档看过了 win7的驱动是正常的能够连接上EV板,目前发现和L4.9.123_2.3.0-ga_images_mx8mm.zip 里面uuu.auto脚本文件的FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard 这句有关系。L4.9.123_2.3.0-ga_images_mx8mm.zip 里面没有.sdcard后缀的文件,只有fsl-image-validation-imx-imx8mmevk.sdcard.bz2  但除了手动解压出.sdcard再执行烧录,还有什么别的方法么?

0 Kudos

2,482 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

About use uuu to download the images to i.MX8M Mini EVK board you can refer to the link.

Get Started with the i.MX 8M Mini EVK | NXP 

And on the window 7 you need to do some modify. You can see the document UUU.pdf

here Releases · NXPmicro/mfgtools · GitHub .
Have a great day,
Rita

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos