Alternate to IAM-82008-TR1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Alternate to IAM-82008-TR1

508 Views
ramakrishnach
Contributor I

We are presently using M/s Agilent Make, IAM-82008-TR1, RF Mixer in our module. This part is no more available from M/s Agilent.

We are presently using this IC in HF Radio, Tx up and Down conversion stages, where the RF freq is in between 1 MHZ to 250 MHz and LO is also in between 1 MHZ to 250 MHz range.

We checked on NXP website, where the model SA602A, is almost meeting the required specifications, however PIN to PIN compatibility is not meeting.

As we already supplied more than 15000 units to our customer, it is difficult to modify board layout.

Please suggest any Functional, Form, Fit Alternate to IAM-82008-TR1.

Labels (1)
  • RF

Tags (1)
0 Kudos
1 Reply

429 Views
LPP
NXP Employee
NXP Employee

NXP doesn't offer pin-to-pin replacement for  IAM-82008-TR1.

SA602A/SA612A are the only functional cross parts.

Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos