Hi members,
I faced the following error when tried to do :- bitbake fsl-image-validation-imx -c populate_sdk in I.Mx8 mini.
Sharing snippet or error found , please provide suggestion's.
Thanks and regards,
Santhosh. K
Hello,
Please check carefully if Your host system meets requirements, mentioned
in section 3 (Host Setup) of the corresponding "i.MX_Yocto_Project_User's_Guide.pdf".
https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS
Also, please use the following general Yocto recommendations regarding host setup,
perhaps some packages on Your host should be updated / upgraded.
(In particular - Python 3.4.0 or greater)
https://www.yoctoproject.org/docs/current/ref-manual/ref-manual.html#detailed-supported-distros
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.