Hello,
the problem is that you send only 'X' but the ZSTAR3 USB Stick wait for full Burst On command 'X' and two bytes more that are used as a 16-bit mask and each bit is used as a enable burst option for individual sensors.
That's all
Have a nice day and good luck
Hi Petr,
I have the same problem. Could you make an example for the Burst mode?
Is there a way to switch off the sleep mode by sending a Zstar command?
Thank you very much.
Best regards.
Dominic
Hello to Switch on Burst mode for all sensors it has to be send to USB Stick this command (in hex) "58FFFF" , but if you want to active burst mode only for fisrt sensor then you have to send "580001".
That's all - first byte is command 'X' andnext two is enable bitmask.
And you second problem - If you want to disable sleep features of ZSTAR3 sensors, then you have to periodically send cammand 'Y' to USB Stick. And USB Stick erase timeout counter in each sensor.
The period for this command I recommend about 30 seconds.
Have a nice day
Thank you very much for your fast reply.
Now it works.
Thanks
Dominic