In Imx6q Security Reference Manual Chapter 6, see following:
If the SNVS determines the chip is in a trustworthy state, it allows CAAM to use a secret 256-bit value that CAAM uses to derive cryptographic keys during blob encapsulation and decapsulation.
We can know CAAM use 256-bit secret value to devrie cryptographic key blob encapsulation and decapsulation.
I want to confim if only CAAM can read this 256-bit secret value from SNVS? If not, except CAAM, who can read this 256-bit secret value from SNVS?
Hello,
I've sent some comments directly.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.