AnsweredAssumed Answered

UART jitter spec at max speed

Question asked by Jake Bailey on Apr 24, 2019
Latest reply on Apr 25, 2019 by Yuri Muhin

What is the tolerable jitter for imx6 UART at max speed of 4mbps?

 

The reference manual makes claims that there are new improvements to voting mechanism triggering that improve performance. Is this already accounted for in datasheet spec? From what I understand datasheet is claiming 6% jitter per bit with max 18% per 9bit word.

 

Our application requires 4mbps at up to 300m so I am trying to decide if RS485 drivers need equalization to reduce jitter or not.

 

Thanks.

Outcomes