iMX8 - SCU ROM Passover information reading

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 - SCU ROM Passover information reading

773 Views
Ansari
Contributor IV

Hi Team,

Currently we are using i.MX8DX6-B0 silicon based custom platform along with 4.14.78 GA BSP release.

We have referred the document https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf

From the above mentioned document "5.12.2 SCU ROM Passover" section explains about SCU ROM passover information(added in attachment). We would like to read the SCU ROM passover information to get the values of the "Image set booted from" field.

We understood that this field will give the information about 1st/2nd Image container set which is booted from.

Could you help us on this.

Thanks and Regards,

Ansari

0 Kudos
2 Replies

661 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ansari

document was provided via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

406 Views
peter82
Contributor I

Could you please provide the document for me as well?

0 Kudos