I am trying to perform recovery on a LS1012A-FRWY that doesn’t boot anymore and I’m following the procedure as described in https://community.nxp.com/thread/439034?commentID=852508#comment-852508.
I am unable to connect to the core, even if I am setting USE_SAFE_RCW=True.
In CW I'm getting the following:
When USE_SAFE_RCW=False, I get this:
Using CLI:
The board does not boot. No characters appear on the terminal.
The onboard K20 works fine, the MBED drive appears, the virtual COM port works and I am able to put the K20 in bootloader.
I am using an external CMSIS-DAP interface connected to J11.
I saw something about the R50 (in several topics; e.g.LS1012A-FRDM Codewarrior Flash Error )
Do I have to perform any hw procedures on the board?
Please advise.
Thank you!
Can this be done using a generic JTAG probe or only with the CodeWarrior TAP?
The recovery could be done by CodeWarrior IDE + CodeWarrior TAP only.
Please consider that in the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.6.2 Program valid RCW in flash device using Flash Programmer there is following note:
"When using the CMSIS-DAP probe, it is recommended to verify operation parameters and RCW correctness before continuing. Failure to program a compatible RCW may result in board being unable to boot. Recovery is not possible using CSMSIS-DAP and will require use of the external CodeWarrior TAP unit".