I'm currently working with the LS1046A-RDB reference board design kit provided by eInfoChips. The application notes on the system defines that the available memory for the single physical bank is 8-GB. For the reference kit, is this the maximum available memory or can I swap the memory module with a larger DDR4?
When designing my own board off the LS1046A QorIQ Layerscape, what's the maximum physical bank count and memory capacity per bank that I can put into my design?
Solved! Go to Solution.
Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.
The DDR controller supports 4 banks.
Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.
Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.
The DDR controller supports 4 banks.
Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.