AnsweredAssumed Answered

For the M8 Mini: Is it possible to generate an MCLK of 12.288MHz internally for use both in the an SAI module and externally for an audio codec, or do I need to generate this frequency externally?

Question asked by Yishai Kagan on Apr 15, 2019
Latest reply on Apr 15, 2019 by igorpadykov

12.288MHz is a common frequency used an the master clock for 48KHz audio streams. It can be generated from 24MHz by a full-blown PLL by placing 125 in the divisor and 64 in the multiplier. It is not clear to me whether this can be done in the M8 Mini.

Outcomes