AnsweredAssumed Answered

UART on i.MX7D A7 core

Question asked by Emiliano Costagli on Apr 9, 2019
Latest reply on Apr 9, 2019 by igorpadykov

Hello people,

Has anybody tried to get the UART working on the Cortex-A7 core of the i.MX7D device, running a baremetal program?

I have started from the FreeRTOS_BSP_1.0.1_iMX7D project, changing the start-up code to run on one of the A7, but I don't seem to be able to access any of the UART interfaces (even from the debugger, the UART registers are either 0 or unreadable). I don't think the problem is in the MMU, because I am configuring it to access the full AIPS ranges.

 

By the way, on the FreeRTOS_BSP_1.0.1_iMX7D project, I believe the base address of the UART2 (UART2_BASE) is wrong: in MCIMX7D_M4.h it is defined as 0x30890000, while, according to the reference manual, it should be 0x30870000.

Thanks,

 

-Emiliano

Outcomes