请问MPL3115A2适用于测量高空气压吗,这个参数什么意思

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

请问MPL3115A2适用于测量高空气压吗,这个参数什么意思

737 Views
1243962643
Contributor I

工作范围:20 kPa至110 kPa绝对压力
校准范围:50 kPa至110 kPa绝对压力

工作和校准有什么区别,20 VS 50

0 Kudos
2 Replies

635 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Within the calibrated pressure range, the accuracy meets the requirements of the specification described in the MPL3115A2 datasheet. If the measured pressure is out of this range, but within the operational pressure range, the sensor still functions reasonably well, but does not meet all accuracy requirements specified in the datasheet.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos

635 Views
1243962643
Contributor I

哦哦,谢谢。

您竟然看的懂中文

0 Kudos