Hi, I need to embed a Sabre board into a fleet of vehicles, can I ask a few questions before doing so?
Thanks for comments
Hi Paul,
The SABRE boards are for evaluation and development purposes, they are not intended to be directly used on end-applications.
All the hardware design documentation is included on the following package:
https://www.nxp.com/webapp/Download?colCode=IMX6SOLOX-SABRESDB-DESIGNFILES&appType=license
This board does not have/require cooling for the targeted purpose (evaluation/development).
The part number of the i.MX processor used on this board is the following:
MCIMX6X4EVM10AB (Extended Commercial product, operative from -20 to 105 °C).
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Hi CarlosCasillas thanks for your reply. Do you have any recommended vendor or industrial designs based on this board?