Moving a Mifare Plus S 2K into SL3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Moving a Mifare Plus S 2K into SL3

687 Views
daniel-alin_ion
Contributor I

Hello,

I'm having issues moving a mifare plus s 2K card into sl3. The personalization was done and the card is now in SL1, all the keys have been written in blocks 0x4000-0x403f, 0x9000-0x9003.

I'm issuing a RATS command to enter t=cl protocol and then a firstauth to 0x9003. I'm correctly getting a challenge from the card, a 16 byte rndB, which I decrypt and rotate.

However, after I issue a following auth with rndA and rndB' the card returns:

00 00 0b 01 06 90 00 instead of rndA' and the rest of needed information.

(using an omnikey, so the first 4 bytes are two zeroes, a PCB and CID and then return code 6).

From what I can see, this error means that the block does not exist or the access conditions are not fulfilled. Might this be an error in how I compose rndA|rndB'? Or is there something else I must do first?

Thanks.

Labels (1)
0 Kudos
1 Reply

536 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies, this information is confidential and cannot be handled on the public community.

Thank you for your comprehension.

Regards,

Ivan.

0 Kudos