Also how can I trigger turn ON of processor from shutdown condition with out using ONOFF switch?
Hello,
If OFF state means all power supply voltages of the i.MX 6ULL, except VDD_SNVS_IN, are OFF, than
it is impossible to assert any signals (except ONOFF) of the i.MX 6ULL in order to activate an external (PMIC)
power supply scheme.
If i.MX 6ULL is completely de-energized, then its PMIC_ON_REQ will be asserted automatically
when VDD_SNVS_IN is applied. This allows to switch on all the rest voltages for i.MX 6ULL
from a PMIC.
Have a great day,
Yuri
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------