I am trying to implement emWin for my IMXRT1050-EVKB board using Keil IDE using an SPI based TFT driver. I just came across emWin GUI Demo available on MCUXpresso SDK v2.5.0 with default path as:
\SDK_2.5.0_EVKB-IMXRT1050\boards\evkbimxrt1050\emwin_examples\emwin_gui_demo\mdk
I would like to know if it is possible to use the same Demo and port the code for my SPI based TFT Display using MCUXpresso.
Regards,
Snehal
Hi Snehal,
yes, you can. You can import demo in SDK into MCUXpresso by clicking the Quick Panel->import SDK example(s)
If you want to port a SPI LCD, you can download a K64 KSDK. There is also a SPI base enWin demo. Since NXP demo and middle share same structure, you can easily know how to porting by compare the two demo.
Regards,
Jing