AnsweredAssumed Answered

重新编译bitbakefsl-image-mfgtool-initramfs

Question asked by changjing chi on Apr 2, 2019
Latest reply on Apr 8, 2019 by jimmychan

大家好!

自己设计的硬件设备使用官方的L4.1.15_1.0.0_ga-mfg-tools下载失败

在uboot跳转到kernel之前打印如下

                                                                                

U-Boot 2015.04-imx_v2015.04_3.14.38_6qp_ga+gf80d628 (Mar 30 2019 - 21:28:42)    

                                                                                

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz                                       

CPU:   Temperature 30 C                                                         

Reset cause: POR                                                                

Board: MX6-SabreSD                                                              

I2C:   ready                                                                    

DRAM:  1 GiB                                                                    

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2                                    

MMC: no card present                                                            

MMC init failed                                                                 

Using default environment                                                       

                                                                                

No panel detected: default to Hannstar-XGA                                      

Display: Hannstar-XGA (1024x768)                                                

In:    serial                                                                   

Out:   serial                                                                   

Err:   serial                                                                   

MMC: no card present                                                            

Net:   FEC [PRIME]                                                              

Error: FEC address not set.                                                     

                                                                                

Boot from USB for mfgtools                                                      

Use default environment for                              mfgtools               

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; 

Hit any key to stop autoboot:  0                                                

Kernel image @ 0x12000000 [ 0x000000 - 0x597278 ]                               

## Loading init Ramdisk from Legacy Image at 12c00000 ...                       

   Image Name:   fsl-image-mfgtool-initramfs-imx6                               

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)                      

   Data Size:    7565864 Bytes = 7.2 MiB                                        

   Load Address: 00000000                                                       

   Entry Point:  00000000                                                       

   Verifying Checksum ... OK                                                    

## Flattened Device Tree blob at 18000000                                       

   Booting using the fdt blob at 0x18000000                                     

   Using Device Tree in place at 18000000, end 1800d51a                         

No PMIC found!                                                                  

                                                                                

Starting kernel ...                                                             

进入kernel之后到这个一步就一直停止,无法识别usb

Starting kernel ...

UTP: Waiting for device to appear                                               

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails                                  

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails                                  

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails                                  

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails                                  

max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails

 

 

现在需要自己修改固件,请问一下有移植手册可以参考么?

Outcomes