S32K144: How to capture all wake-up source when exiting the VLPS mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144: How to capture all wake-up source when exiting the VLPS mode

1,514 Views
dsfire
Contributor III

Hi, all,

I use function INT_SYS_DisableIRQ(xx) to disable all interrupt (IRQ num >=0 && IRQ num <=122) except PORTA_IRQn, PORTB_IRQn, PORTC_IRQn, PORTD_IRQn, PORTE_IRQn before executed function POWER_SYS_SetMode(VLPS, POWER_MANAGER_POLICY_AGREEMENT), and use function PORT_HAL_GetPortIntFlag(xx) to capture the port interrupt flag in ISR of PORTA~PORET.

But, nothing flag (print to uart) can be captured sometimes when exiting VLPS mode.

So, how to capture all wake-up source when exiting the VLPS mode?

Regards,

Liu

0 Kudos
3 Replies

1,178 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Liu,

If I understand, the MCU can wake up without any problem but you can't capture the source of the interrupt.

Something similar was discussed here:

https://community.nxp.com/thread/493555

Instead of PORT_HAL_GetPortIntFlag(xx), you can use this:

pastedImage_1.png

Regards,

Daniel

0 Kudos

1,178 Views
dsfire
Contributor III

Hi,

Daniel,

Thanks for your response.

What's the different between PORT_HAL_GetPortIntFlag and PINS_DRV_GetPortIntFlag, because there is no function PINS_DRV_GetPortIntFlag in my pins_driver.c file.

And here is the implementation of function PORT_HAL_GetPortIntFlag:

static inline uint32_t PORT_HAL_GetPortIntFlag(const PORT_Type* const base)
{
    uint32_t regValue = base->ISFR;
    return regValue;
}

 

Regards,

Liu

0 Kudos

1,178 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Liu,

Sorry, both the functions do actually the same thing.

You probably use an old version of the SDK.

I took the screenshot from the SDK RTM 3.0.0 documentation which can be found in the installation folder of the SDK.

...\NXP\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_RTM_3.0.0\doc\Start_here.html

If you start a new project, I would recommend the current SDK version.

Regards,

Daniel

0 Kudos