We are currently evaluating the performance of the imx8 family of processors. We found the CPU and GPU performance parameters for imx8 and imx8m, but for the imx8x and imx8m mini series, we were unable to find the relevant parameters.
E.g:
i.MX 8QuadMax | i.MX 8QuadPlus | i.MX 8DualMax | |
CPU | 2xA72+4xA53 | 1xA72+4xA53 | 2xA72 |
DMIPS | 26k | 18.5k | 15k |
GPU | 2x GC7000 XSVX | 2x GC7000Lite XSVX | 1x GC7000 XSVX |
GFLOPS | 128 | 80 | 64 |
i.MX 8MQuad | i.MX 8MQuadLite | i.MX 8Dual | |
CPU | 4xA53 | 4xA53 | 2xA53 |
DMIPS | 13.8k | 13.8k | 6.9k |
GPU | GC7000Lite | GC7000Lite | GC7000Lite |
GFLOPS | 64 | 64 | 64 |
1. What is the DMIPS of the CPU of the imx8x (8qxp, 8dxp, 8dx) series, and what is the GFLOP of the GPU?
2. What is the DMIPS of the CPU of the imx8m mini (Mini Quad, Mini Dual, Mini Solo) series, and what is the GFLOP of the GPU?
Hi Jinlong,
Unfortunately, we do not have any performance data that we can share, please contact your NXP Sales/FAE regarding these features, they would be able to help you.
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------