I.MXRT1064 : How to access Internal Flash for read/write operation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MXRT1064 : How to access Internal Flash for read/write operation?

1,163 Views
vishaldahiwal
Contributor II

I need to access the internal flash to store the downloaded image from server.

Internal 4 MB Flash to be partitioned in three sections as shown below,

  1. Currently executing image. This image will download the other image from server.
  2. Downloaded image.
  3. User Data

Here, I am looking for the mechanism to access the second partition of internal flash from first partition (i.e. code executing from partition 1).

Currently I am using the I.MXRT1064EVK board and downloaded the sample code flexspi_nor_polling_transfer from SDK. This code is for accessing the external flash connected to FLEXSPI1.

I need the example code which can access (Read/Write/Erase) the internal 4MB flash (internally connected to FLEXSPI2) from program executing from address 0x7000_0000.

I tried modifying the flexspi_nor_polling_transfer to use FLEXSPI2 but it is not working.

Now I have following questions,

1. Can flexspi_nor_polling_transfer be modified to access internal 4MB flash?

2. Is there any code which I can use in program executing from 0x7000_0000 (e.g. emwin_gui_demo) to access any memory (outside of the current executing program area) of internal flash?

Labels (1)
0 Kudos
1 Reply

813 Views
carstengroen
Senior Contributor II

vishaldahiwal@gmail.com‌,

you might get some ideas from here: https://community.nxp.com/thread/498852 

0 Kudos