Hello,
I've a new project by using SKEAZN32.And I want to created LDF and NPF file then generateing "lin_cfg.c" files by tool,I try to use S32Ds and KDS to do this job,but it doesn't work.So i want to know if are there some ways to generate "lin_cfg.c" files by tools.If so, what should I do.
Thanks.
Hi jiaqi Shen,
I recommend you to check the following application note in chapter 4.1:
Using NXP’s LIN Driver with the MagniV Family
For this you will need to download the NXP LIN Driver Package from the following link:
LIN2.x and SAE J2602 Stack
Please keep in mind that this driver is using CodeWarrior and you will need to install the plug-in in order to create LDF and NPF files (check chapter 3.1 of Eclipse_User_Manual inside the NXP LIN Driver installation folder).
I hope this helps you.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------