Hi,
When i.MXRT1050 connect to LCD, how to set DOT clock of LCD?
Does dot clock is direct to connect LCDIF_CLK_ROOT?
Is there any clock divider between LCDIF_CLK_ROOT to DOT clock?
Best Regards,
Sugiyama
Hi,
When i.MXRT1050 connect to LCD, how to set DOT clock of LCD?
Does dot clock is direct to connect LCDIF_CLK_ROOT?
Is there any clock divider between LCDIF_CLK_ROOT to DOT clock?
Best Regards,
Sugiyama
You can set the DOT clock refer to the reference manual.The LCD_DOTCLK is max 75MHz, see LCDIF_CLK_ROOT in Reference Manual. And defult the value of the divider is 1 between with LCDIF_CLK_ROOT to DOT clock. Hope it help you.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi, TIC team,
Thank you for your answer.
I' not sure which divider are you specified LCDIF_CLK_ROOT to DOT clock?
I can see LCDIF_PODF(default=1/4), and LCDIF_PRED(default=1/4), but I couldn't find the other register for LCDIF clock.
Could you specify the register name?
Best Regards,
Sugiyama
Hello,
Unfortunately, I can't find the other register for LCKIF clock. But the DOT clock please refer to the document. URL:https://www.nxp.com/docs/en/application-note/AN12302.pdf.
Hello,
Unfortunately, I can't find the other register for LCKIF clock. But the DOT clock please refer to the document. URL:https://www.nxp.com/docs/en/application-note/AN12302.pdf.