AnsweredAssumed Answered

Question for the Number of images that can be simultaneously decoded in i.MX8MQ

Question asked by Eric Kang on Mar 26, 2019
Latest reply on Apr 15, 2019 by Rita Wang

Dear All,

 

I want to know the Number of images that can be simultaneously decoded in i.MX8MQ.
Could you tell me the number?

 

Our test environment is like as below.
For Video Display, we have to make the One-Display image with 4-channels or 8-channels.
So we need to check the Number of images that can be simultaneously decoded in i.MX8MQ.

 

- MPU : i.MX8MQ
- Video Input
  . Interface : Gigabit Ethernet
  . Encoding : H.264 or H.265
  . Video Resolution : No Fixed
- Video Save
  . Interface : PCIe for HDD/SDD
- Video Output
  . Image : One Display with 4-channel or 8-channel
  . Interface : HDMI / 4K(4096x2160)@60Hz
  . Video Resolution : 4K(4096x2160)@60Hz

 

- Block Diagram

  .

 

Best Regards,
Eric.

Outcomes