AnsweredAssumed Answered

Question Regarding VSUP pin implementation in Magni V

Question asked by kunmit patra on Mar 25, 2019
Latest reply on Mar 26, 2019 by Daniel Martynek

I am using 'MC9S12ZVHY' series MagniV Microcontroller. Need to monitor the Analog voltage range from 0 to 5 V. 

I am using the VSUP pin for this purpose which can be routed to internal ADC through an Internal Voltage Divider.

 

The VSUP pin has following characteristics :

i Am confused with the above mentioned Condition " 5.5V < VSUP < 29 V" .

My Question is:

Can i use the VSUP pin as internal ADC to Measure analog voltage from 0 to 5V Range?

 

Please help me on this issue.

 

Thanks

Kunmit

Outcomes