Hi,
What's the minimum supply voltage for the MML09212H? If I power it with 4.5V for exemple, should I expect a big difference in terms of performance?
Thank you,
Kind regards.
Hi,
It is not recommended to supply the MML09212H with a different voltage than 5.0V as this device is only characterized to operate with this voltage supply level.
If a different voltage is used, NXP cannot warranty the proper performance of the device.
Have a great day,
Jose
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------