大家好,
我用的芯片为imx6solo, BSP为yocto L4.1.15-2.1.0。
目前使用SD卡和micro SD卡启动时出现很奇怪的现象。根据《i.MX_Linux_User's Guide.pdf》文件对SD卡和micro SD卡进行分区,格式化,然后烧写同样的u-boot.imx,zImage,设备树,文件系统。在启动时,SD卡可以正常启动到文件系统,但是使用micro SD卡插上卡套,然后启动时,就只能启动到uboot,到kernel阶段就报错,如下log。另外,我仔细对比了两个SD卡的状态,使用df -h和fdisk -l查看了,基本都是一样的,请教各位大神帮助,谢谢。
U-Boot 2016.03-svn1773 (Mar 22 2019 - 14:30:42 +0800)
CPU: Freescale i.MX6SOLO rev1.2 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 59C
Reset cause: POR
Board: MX6SOLO RIoTboard
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
config_ipu_di_clk: freq = 148500000.
wait for pll5 lock.
config_ipu_di_clk: set pll5 clock to 294000000Hz.
switch to partitions #0, OK
mmc0 is current device
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
switch to partitions #0, OK
mmc0 is current device
reading zImage
6093216 bytes read in 294 ms (19.8 MiB/s)
Booting from mmc ...
reading imx6solo_mehowboard.dtb
33830 bytes read in 19 ms (1.7 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x5cf9a0 ]
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800b425
Starting kernel ...
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
random: nonblocking pool is initialized
Do you mean you are inserting SD and microSD into the same slot (microSD with an adapter).
There should be no difference.
Maybe one of them is a bit instable, please try another one (for example another brand).
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thank you very much, the problem has been solved