Is it possible to use OM5578/PN7150 with Arduino

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to use OM5578/PN7150 with Arduino

1,540 Views
a_feil
Contributor I

I would like to use the PN7150 NFC Controller board on an Arduino (model is not important). Is there a guide/library for the arduino  IDE?

Tags (3)
0 Kudos
2 Replies

1,039 Views
eschwartz
Contributor I

I want to add my voice to the chorus wondering about (non-existent) PN7120/7150 support for Arduino / non-ST parts.

It's particularly interesting because ST produces the OM5578 -- was really hoping they'd put together a library for Arduino, but just seems to be leveraging the header which is common to other platforms.

0 Kudos

1,039 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the NXP-NCI example projects for MCUXPresso IDE. They are only available for our MCUs but you could take them as a reference.

Have a nice day.

Regards,

Ivan.

0 Kudos