Analog voltage comparator not working on i.MXRT1062

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Analog voltage comparator not working on i.MXRT1062

Jump to solution
1,540 Views
rohit_ballurgi
Contributor III

I am trying to compare voltages using comparator 1 and 2 for the power inputs GPIO_AD_B1_02 (usb) & GPIO_AD_B1_03 (board) on my i.MXRT1062 hardware. It is not working. I am using continuous mode. I'm powering the device from both the power inputs. When I remove one of the power inputs, I'm expecting the interrupt to be hit, but it is not hitting.

 

CMP1

#define DEMO_CMP_BASE CMP1

#define DEMO_CMP_USER_CHANNEL 3U

#define DEMO_CMP_DAC_CHANNEL 7U

#define DEMO_CMP_IRQ_ID ACMP1_IRQn

#define DEMO_CMP_IRQ_HANDLER_FUNC ACMP1_IRQHandler

 

mCmpDacConfigStruct.referenceVoltageSource = kCMP_VrefSourceVin2; /* VCC. */

mCmpDacConfigStruct.DACValue = 32U;                                /* Half voltage of logic high level. */

 

CMP2

#define DEMO_CMP_BASE CMP2

#define DEMO_CMP_USER_CHANNEL 3U

#define DEMO_CMP_DAC_CHANNEL 7U

#define DEMO_CMP_IRQ_ID ACMP2_IRQn

#define DEMO_CMP_IRQ_HANDLER_FUNC ACMP2_IRQHandler

 

mCmpDacConfigStruct.referenceVoltageSource = kCMP_VrefSourceVin1; /* VCC. */

mCmpDacConfigStruct.DACValue = 32U;                                /* Half voltage of logic high level. */

1 Solution
1,391 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi robit ballurgi,

   Today, I test the GPIO_AD_B1_02 on my side, it works OK, I use the SDK code, the board is the RT1060-EVKB.

The SDK code project folder is:

SDK_2.5.0_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\cmp\interrupt\iar

Now, just take GPIO_AD_B1_02, CMP1, channel 3 as an example, the modify point:

1. pin_mux.c, add these code:

  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B1_02_GPIO1_IO18,        /* GPIO_AD_B1_01 is configured as GPIO1_IO17 */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
    
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B1_02_GPIO1_IO18,        /* GPIO_AD_B1_01 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */

2. cmp_interrupt.c

#define DEMO_CMP_USER_CHANNEL 3U
//#define DEMO_CMP_USER_CHANNEL 0U

Then, test:

    - CMP1_IN3 (J22-7) connected to VCC =3.3V (J24-8): USER LED on
    - CMP1_IN3 (J22-7) connected to GND (J24-7): USER LED off

The function works OK.

I find you didn't add this code:

  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B1_02_GPIO1_IO18,        /* GPIO_AD_B1_01 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */

So, please try it again.

GPIO_AD_B1_03 is the same, you can try it.

If you still have question about it, please kindly let me know.

 

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
8 Replies
1,392 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi robit ballurgi,

   Today, I test the GPIO_AD_B1_02 on my side, it works OK, I use the SDK code, the board is the RT1060-EVKB.

The SDK code project folder is:

SDK_2.5.0_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\cmp\interrupt\iar

Now, just take GPIO_AD_B1_02, CMP1, channel 3 as an example, the modify point:

1. pin_mux.c, add these code:

  IOMUXC_SetPinMux(
      IOMUXC_GPIO_AD_B1_02_GPIO1_IO18,        /* GPIO_AD_B1_01 is configured as GPIO1_IO17 */
      0U);                                    /* Software Input On Field: Input Path is determined by functionality */
    
  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B1_02_GPIO1_IO18,        /* GPIO_AD_B1_01 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */

2. cmp_interrupt.c

#define DEMO_CMP_USER_CHANNEL 3U
//#define DEMO_CMP_USER_CHANNEL 0U

Then, test:

    - CMP1_IN3 (J22-7) connected to VCC =3.3V (J24-8): USER LED on
    - CMP1_IN3 (J22-7) connected to GND (J24-7): USER LED off

The function works OK.

I find you didn't add this code:

  IOMUXC_SetPinConfig(
      IOMUXC_GPIO_AD_B1_02_GPIO1_IO18,        /* GPIO_AD_B1_01 PAD functional properties : */
      0x10B0u);                               /* Slew Rate Field: Slow Slew Rate
                                                 Drive Strength Field: R0/6
                                                 Speed Field: medium(100MHz)
                                                 Open Drain Enable Field: Open Drain Disabled
                                                 Pull / Keep Enable Field: Pull/Keeper Enabled
                                                 Pull / Keep Select Field: Keeper
                                                 Pull Up / Down Config. Field: 100K Ohm Pull Down
                                                 Hyst. Enable Field: Hysteresis Disabled */

So, please try it again.

GPIO_AD_B1_03 is the same, you can try it.

If you still have question about it, please kindly let me know.

 

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,391 Views
rohit_ballurgi
Contributor III

Hi Kerry,

It is working now. A resistor connecting the voltage sense to the controller was missing. I appreciate your support. Thank you.

Regards,

Rohit

0 Kudos
1,391 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Rohit,

    That's very good to hear you make it work now.

    If you still have question about it, please kindly let me know.

    If your question is solved, please help me to mark the correct answer, just to close this case, thank you!


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,391 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi robit ballurgi,

    Do you test it with the SDK code?

    Do you configure the pin in the pin_mux.c for your GPIO_AD_B1_02  and GPIO_AD_B1_03?

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,391 Views
rohit_ballurgi
Contributor III

Hi Kerry,

Yes. I'm using SDK example code. And I have configured these pins.

Regards,

Rohit

0 Kudos
1,391 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Robit,

   Please also share your pin mux code, I need to check it.

   You also can upload your problem project, then I will help you to test it on my side.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,391 Views
rohit_ballurgi
Contributor III

I have shared my project on google drive. Please check this link.

test_base_proj.zip - Google Drive 

0 Kudos
1,391 Views
rohit_ballurgi
Contributor III

Hi Kerry,

PSB for my mux config. How you want me to share my project?

void BOARD_InitPins(void) {
CLOCK_EnableClock(kCLOCK_Iomuxc); /* iomuxc clock (iomuxc_clk_enable): 0x03u */

IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_B0_00_GPIO1_IO00, /* GPIO_AD_B0_00 is configured as GPIO1_IO00 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_B0_12_LPUART1_TX, /* GPIO_AD_B0_12 is configured as LPUART1_TX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_B0_13_LPUART1_RX, /* GPIO_AD_B0_13 is configured as LPUART1_RX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_B1_02_GPIO1_IO18, /* GPIO_AD_B1_02 is configured as GPIO1_IO18 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_B1_03_GPIO1_IO19, /* GPIO_AD_B1_03 is configured as GPIO1_IO19 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_B1_09_GPIO1_IO25, /* GPIO_AD_B1_09 is configured as GPIO1_IO25 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B0_05_GPIO2_IO05, /* GPIO_B0_05 is configured as GPIO2_IO05 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B0_06_GPIO2_IO06, /* GPIO_B0_06 is configured as GPIO2_IO06 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B0_07_GPIO2_IO07, /* GPIO_B0_07 is configured as GPIO2_IO07 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B0_08_GPIO2_IO08, /* GPIO_B0_08 is configured as GPIO2_IO08 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B0_11_GPIO2_IO11, /* GPIO_B0_11 is configured as GPIO2_IO11 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_00_LPUART4_TX, /* GPIO_B1_00 is configured as LPUART4_TX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_01_LPUART4_RX, /* GPIO_B1_01 is configured as LPUART4_RX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_04_LPSPI4_PCS0, /* GPIO_B1_04 is configured as LPSPI4_PCS0 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_05_LPSPI4_SDI, /* GPIO_B1_05 is configured as LPSPI4_SDI */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_06_LPSPI4_SDO, /* GPIO_B1_06 is configured as LPSPI4_SDO */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_07_LPSPI4_SCK, /* GPIO_B1_07 is configured as LPSPI4_SCK */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_B1_08_GPIO2_IO24, /* GPIO_B1_08 is configured as GPIO2_IO24 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_01_GPIO4_IO01, /* GPIO_EMC_01 is configured as GPIO4_IO01 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_04_GPIO4_IO04, /* GPIO_EMC_04 is configured as GPIO4_IO04 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_09_GPIO4_IO09, /* GPIO_EMC_09 is configured as GPIO4_IO09 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_10_GPIO4_IO10, /* GPIO_EMC_10 is configured as GPIO4_IO10 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_12_GPIO4_IO12, /* GPIO_EMC_12 is configured as GPIO4_IO12 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_13_LPUART3_TX, /* GPIO_EMC_13 is configured as LPUART3_TX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_14_LPUART3_RX, /* GPIO_EMC_14 is configured as LPUART3_RX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_15_GPIO4_IO15, /* GPIO_EMC_15 is configured as GPIO4_IO15 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_16_GPIO4_IO16, /* GPIO_EMC_16 is configured as GPIO4_IO16 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_17_GPIO4_IO17, /* GPIO_EMC_17 is configured as GPIO4_IO17 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_22_FLEXSPI2_A_SS1_B, /* GPIO_EMC_22 is configured as FLEXSPI2_A_SS1_B */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_23_GPIO4_IO23, /* GPIO_EMC_23 is configured as GPIO4_IO23 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_25_FLEXSPI2_A_SCLK, /* GPIO_EMC_25 is configured as FLEXSPI2_A_SCLK */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_26_FLEXSPI2_A_DATA00, /* GPIO_EMC_26 is configured as FLEXSPI2_A_DATA00 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_27_FLEXSPI2_A_DATA01, /* GPIO_EMC_27 is configured as FLEXSPI2_A_DATA01 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_28_FLEXSPI2_A_DATA02, /* GPIO_EMC_28 is configured as FLEXSPI2_A_DATA02 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_29_FLEXSPI2_A_DATA03, /* GPIO_EMC_29 is configured as FLEXSPI2_A_DATA03 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_30_GPIO4_IO30, /* GPIO_EMC_30 is configured as GPIO4_IO30 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_31_GPIO4_IO31, /* GPIO_EMC_31 is configured as GPIO4_IO31 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_33_GPIO3_IO19, /* GPIO_EMC_33 is configured as GPIO3_IO19 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_36_GPIO3_IO22, /* GPIO_EMC_36 is configured as GPIO3_IO22 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_39_GPIO3_IO25, /* GPIO_EMC_39 is configured as GPIO3_IO25 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_40_GPIO3_IO26, /* GPIO_EMC_40 is configured as GPIO3_IO26 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_EMC_41_GPIO3_IO27, /* GPIO_EMC_41 is configured as GPIO3_IO27 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_02_GPIO3_IO14, /* GPIO_SD_B0_02 is configured as GPIO3_IO14 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_04_LPUART8_TX, /* GPIO_SD_B0_04 is configured as LPUART8_TX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B0_05_LPUART8_RX, /* GPIO_SD_B0_05 is configured as LPUART8_RX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_GPR->GPR26 = ((IOMUXC_GPR->GPR26 &
(~(IOMUXC_GPR_GPR26_GPIO_MUX1_GPIO_SEL_MASK))) /* Mask bits to zero which are setting */
| IOMUXC_GPR_GPR26_GPIO_MUX1_GPIO_SEL(0x00u) /* GPIO1 and GPIO6 share same IO MUX function, GPIO_MUX1 selects one GPIO function: 0x00u */
);
IOMUXC_GPR->GPR27 = ((IOMUXC_GPR->GPR27 &
(~(IOMUXC_GPR_GPR27_GPIO_MUX2_GPIO_SEL_MASK))) /* Mask bits to zero which are setting */
| IOMUXC_GPR_GPR27_GPIO_MUX2_GPIO_SEL(0x01000800u) /* GPIO2 and GPIO7 share same IO MUX function, GPIO_MUX2 selects one GPIO function: 0x01000800u */
);
IOMUXC_GPR->GPR28 = ((IOMUXC_GPR->GPR28 &
(~(IOMUXC_GPR_GPR28_GPIO_MUX3_GPIO_SEL_MASK))) /* Mask bits to zero which are setting */
| IOMUXC_GPR_GPR28_GPIO_MUX3_GPIO_SEL(0x00u) /* GPIO3 and GPIO8 share same IO MUX function, GPIO_MUX3 selects one GPIO function: 0x00u */
);
IOMUXC_GPR->GPR29 = ((IOMUXC_GPR->GPR29 &
(~(IOMUXC_GPR_GPR29_GPIO_MUX4_GPIO_SEL_MASK))) /* Mask bits to zero which are setting */
| IOMUXC_GPR_GPR29_GPIO_MUX4_GPIO_SEL(0x031000u) /* GPIO4 and GPIO9 share same IO MUX function, GPIO_MUX4 selects one GPIO function: 0x031000u */
);
IOMUXC_SetPinConfig(
IOMUXC_GPIO_AD_B0_12_LPUART1_TX, /* GPIO_AD_B0_12 PAD functional properties : */
0x10B0u); /* Slew Rate Field: Slow Slew Rate
Drive Strength Field: R0/6
Speed Field: medium(100MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_AD_B0_13_LPUART1_RX, /* GPIO_AD_B0_13 PAD functional properties : */
0x10B0u); /* Slew Rate Field: Slow Slew Rate
Drive Strength Field: R0/6
Speed Field: medium(100MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */

IOMUXC_SetPinConfig(
IOMUXC_GPIO_EMC_22_FLEXSPI2_A_SS1_B, /* GPIO_SD_B1_06 PAD functional properties : */
0x10F1u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0/6
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_EMC_25_FLEXSPI2_A_SCLK, /* GPIO_SD_B1_07 PAD functional properties : */
0x10F1u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0/6
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_EMC_26_FLEXSPI2_A_DATA00, /* GPIO_SD_B1_08 PAD functional properties : */
0x10F1u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0/6
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_EMC_27_FLEXSPI2_A_DATA01, /* GPIO_SD_B1_09 PAD functional properties : */
0x10F1u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0/6
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_EMC_28_FLEXSPI2_A_DATA02, /* GPIO_SD_B1_10 PAD functional properties : */
0x10F1u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0/6
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_EMC_29_FLEXSPI2_A_DATA03, /* GPIO_SD_B1_11 PAD functional properties : */
0x10F1u); /* Slew Rate Field: Fast Slew Rate
Drive Strength Field: R0/6
Speed Field: max(200MHz)
Open Drain Enable Field: Open Drain Disabled
Pull / Keep Enable Field: Pull/Keeper Enabled
Pull / Keep Select Field: Keeper
Pull Up / Down Config. Field: 100K Ohm Pull Down
Hyst. Enable Field: Hysteresis Disabled */

}

Regards,

Rohit

0 Kudos