HDMI_VP and HDMI_VPH Unused Guidline

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI_VP and HDMI_VPH Unused Guidline

575 Views
markwilliams
Senior Contributor I

Hi,

In the hardware design guidelines it recommends that HDMI_VP and HDMI_VPH are grounded if not used.

In our design we may populate the HDMI feature for some boards and not for others. Is it ok to keep the HDMI_VP and HDMI_VPH pins powered when not used? I would prefer this over trying to fit in a series 0R link to disconnect the supply and then populate a cap footprint with 0R to ground the pins.

Presumably this recommendation is to save powering the HDMI interface when not used, thus reducing power? Is it "safe" to keep these pins powered against the recommendations in the development guide?

Thanks,

Mark

Labels (1)
0 Kudos
1 Reply

342 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mark

you are right, this recommendation is to save overall power consumption

when HDMI interface is not used. Also one can keep these pins powered even HDMI

is not used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos