AnsweredAssumed Answered

Display support

Question asked by Subhan Habib on Mar 19, 2019
Latest reply on Mar 19, 2019 by Subhan Habib

I'm using the Android Things Starter Kit with the PICO-PI-iMX7 board and the included 5" display.

 

I'm looking to get a larger display but I'm not entirely sure what the compatibility is. The included display uses an FPC connector (I think?), here's a link to it: https://shop.technexion.com/tdp0500t800480pcap.html

 

The board lists compatibility for two types of displays:

- 24-bit TTL RGB signals

- MIPI DSI on a 33-pin FPC connector

 

How would I know if the display is compatible? Do all TTL displays come with the same connector size/compatibility? Or is it like the FPC connector which seems to vary in size? Is there any way to use a standard HDMI monitor?

 

Thank you

Outcomes