Hi Support,
GitHub - boundarydevices/linux-imx6 at boundary-imx_4.1.15_2.0.0_ga
We have already used spi-imx.c patch in attach github, however, this issue still happen when traffic are passing throughput SPI interface. Do you have any idea what we encountered ? Thanks a lot !
It looks like error in PIO not DMA...
nrc-cspi spi2.0: I/O Error in PIO
spi_master spi2: failed to transfer one message from queue
Regards,
Steven Yu
Hi Steven
issues for boundary devices software can be posted on its forum:
alternatively one can try with nxp linux releases from source.codeaurora.org/external/imx/linux-imx repository
Linux documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------