imx6qdlsabresd / thud : cannot boot generated wic image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6qdlsabresd / thud : cannot boot generated wic image

1,053 Views
jean-michael_ce
Contributor I

Hello,

I have done the following procedure to try to build an image for my i.MX6 :

- get the fsl-community-bsp repository on branch thud

- run setup-environment like this :

    MACHINE=imx6qdlsabresd DISTRO=fslc-framebuffer ./setup-environment build

- bitbake core-image-minimal

- put the built image on a sd card with wic

The sdcard goes to uboot, but isn't able to boot the linux kernel afterwards (it hangs at "Decompressing kernel..." from what I can see).

I also tried with fsl-image-machine-test with the same result.

Would anyone know what is going wrong ? The card boots fine with the official freescale BSP.

Labels (2)
Tags (2)
0 Kudos
2 Replies

799 Views
art
NXP Employee
NXP Employee

Try to follow exactly the procedure, described in the attached documents. First, refer to the i.MX Yocto Project User's Guide document. Then, follow the i.MX Linux User's Guide document, especially, its "Booting Linux OS" section.

Best Regards,

Artur

0 Kudos

799 Views
jean-michael_ce
Contributor I

For more information, here are my variables :

Build Configuration:

BB_VERSION = "1.40.0"

BUILD_SYS = "x86_64-linux"

NATIVELSBSTRING = "universal"

TARGET_SYS = "arm-fslc-linux-gnueabi"

MACHINE = "imx6qdlsabresd"

DISTRO = "fslc-framebuffer"

DISTRO_VERSION = "2.6"

TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"

TARGET_FPU = "hard"

meta meta-poky = "HEAD:f5a57e939e626a5b7c6de5b51799ca602ed355ed"

meta-oe meta-multimedia = "HEAD:6ef9657068492d4644079c88f2adee9c3cac9543"

meta-freescale = "HEAD:6a43f14bce556189cb8e7338148b777ca6f6141a"

meta-freescale-3rdparty = "HEAD:815df63f9b8997623fe9e23c78de736c25f0a4fd"

meta-freescale-distro = "HEAD:ef7e7ec8141c5099ba87c766108f698b9cc2e9a0"

0 Kudos