AnsweredAssumed Answered

fsl-image-validation-imx.bb.do_build is tainted from a forced run

Question asked by Santhosh Kumar on Mar 12, 2019
Latest reply on Mar 14, 2019 by Bio_TICFSL

Hi,

I am getting the below error while doing yocto build, Please advice how to resolve this issues

 

 

$bitbake fsl-image-validation-imx
Loading cache: 100% |############################################################################################################| Time: 0:00:00
Loaded 3070 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

 

Build Configuration:
BB_VERSION        = "1.32.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-16.04"
TARGET_SYS        = "aarch64-poky-linux"
MACHINE           = "imx8qm_iwg27m"
DISTRO            = "fsl-imx-x11"
DISTRO_VERSION    = "4.9.51-mx8-beta"
TUNE_FEATURES     = "aarch64"
TARGET_FPU        = ""
meta              
meta-poky         = "HEAD:ef888dd58f431866db2472753643f3f848fece21"
meta-oe           
meta-multimedia   = "HEAD:b40116cf457b88a2db14b86fda9627fb34d56ae6"
meta-freescale    = "HEAD:05681fdf8298bb441c15135eae424c7601b07e98"
meta-freescale-3rdparty = "HEAD:e55167c3c2770c07a475342f99cc2a3a23fbfa0c"
meta-freescale-distro = "HEAD:cd5c7a2539f40004f74126e9fdf08254fd9a6390"
meta-bsp          
meta-sdk          = "HEAD:e28cadd7e50cbaeb66d18f8e68e0ffb0a81130c3"
meta-browser      = "HEAD:678706cb43fb8576ff7b88bfb612993b8542724d"
meta-gnome        
meta-networking   
meta-python       
meta-filesystems  = "HEAD:b40116cf457b88a2db14b86fda9627fb34d56ae6"
meta-qt5          = "HEAD:ff073f04109900fc07bf81e2f1df63c626caf342"

 

WARNING: /home/santhosh/Desktop/iwg27-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb.do_build is tainted from a forced run
Initialising tasks: 100% |#######################################################################################################| Time: 0:00:13
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 7548 tasks of which 7548 didn't need to be rerun and all succeeded.

 

Summary: There was 1 WARNING message shown.

 

Regards

Santhosh

Outcomes