AnsweredAssumed Answered

i.MX8M processor pins pull-up /down configuration

Question asked by NIRMAL LUHANA on Feb 12, 2019
Latest reply on Mar 11, 2019 by NIRMAL LUHANA
Branched from an earlier discussion

Hello gusarambula,

 

Thanks for your response.

 

As I gone through the datashhet from the link in last reply there is pins going in PD with 90K at reset time. But after reset condition if i set bits to pull-up enabled then it is going in pull-up condition using 90K or 27K value resistors.

 

Is my understanding correct? or I have to provide external pull-up resistors?

 

Best regards,

Nirmal

Outcomes