AnsweredAssumed Answered

MIMXRT1062CVL5A Alternative Connection For FLASH: How to access?

Question asked by Thomas Monthei on Mar 8, 2019
Latest reply on Mar 13, 2019 by Jing Pan

I have a custom design using an MIMXRT1062CVL5A processor connected to a Winbond FLASH (W25N01GVZEIG) using the following connections:

 

FlexSPI_D3_B                [L5] GPIO_SD_B1_00
FlexSPI_D2_B                [M5] GPIO_SD_B1_01
FLEXSPI_B_SS0_B       [H2] GPIO_SD_B0_04
FlexSPI_D0_B                [M4] GPIO_SD_B1_03
FlexSPI_CLK_B              [P2] GPIO_SD_B1_04
FlexSPI_D1_B                [M3] GPIO_SD_B1_02

 

This configuration is different from the EVK board but seems allowable according to the reference manual. My question is: Is it possible to connect to this board using the PE Micro debugger and drop code onto this FLASH given it's location being different from the EVK board? How do I specify where this FLASH device is connected so that the debugger can find it? 

 

Thanks!

Outcomes