Imx8qxpmek board not booting up properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8qxpmek board not booting up properly

526 Views
krishnan_ramesh
Contributor III

Hi,

I am using i.MX 8QuadXPlus MEK CPU Board. i am trying to flash board using yocto project source code .

Image :fsl-image-validation-imx-xwayland-imx8qxpmek.sdcard image by following command. (referred the manual)

sudo dd if=fsl-image-validation-imx-xwayland-imx8qxpmek.sdcard of=/dev/sdb bs=1M conv=fsync

Sdcard partition (Boot partition and rootfs) is created and all the files are copied into it ,but the board is not booting up and i don't see any boot logs

DIP switches are set to SD card boot

I am unable to figure it out what is causing the issue.

0 Kudos
1 Reply

398 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ramesh,

Check, If you are booting for SD1 the SW2  D1,D2 must be ON D3,D4 OFF.  if you are on eMMC D3 must be ON all rest

OFF.

Thanks

0 Kudos