AnsweredAssumed Answered

S32K ADC

Question asked by Koorosh Hajiani on Mar 6, 2019
Latest reply on Mar 7, 2019 by Petr Stancik

Hi,

Here is the situation:

I've 5 ADC input, 2 are on ADC0 and 3 are on ADC1.

I used PDB0 and PDB1 to convert those 5 channels successfully however now the customer requirement is that 1 input on ADC1 needs to be sampled every 1 ms.  previously all the 5 channels were sampled at 20 ms .

 

So since only SC1_A could be triggered and the rest would follow in a back2back fashion, is this even possible?

if I trigger on the desired input every 1ms and still needs to sample the other 2 in 20ms how is this possible?

 

Thanks,

Koorosh Hajiani

Outcomes