SRK table generation with HSM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRK table generation with HSM

812 Views
rohith_chinnasw
Contributor II

We are using the CST tools 3.1.0 version and have customized the backend to sign the bootloader HAB images. But as part of it the input to the signing process is an SRK table bin file and it looks to be using the private keys to generate it. Since we have the private keys in the HSM is it possible with CST tool to use the HSM backend for the SRK table generation as well?

Labels (1)
Tags (3)
0 Kudos
2 Replies

708 Views
PramodKumar
Contributor IV

Hello Rohith chinnaswamy ,

Are you doing the code signing with imx6ul or any other .

Have a great day ,

Pramod

0 Kudos

708 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

     Please look at  "cst-3.1.0.tar\release\code\back_end-hsm\doc\" .

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos