i.MX28 NAND speeds slow, how to speed up?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX28 NAND speeds slow, how to speed up?

805 Views
manuelbessler
Contributor I

What read/write speeds should I expect from the i.MX28 NAND?

I'm only seeing between 1-2MB/sec which seems very slow. Read/write speeds from/to SD Card are quite a bit faster.

I've tried bumping up the GPMI clock from the default 24MHz to 48MHz and higher. The max speed increase was around 10%. This was with kernel version 4.10 and 4.19.

I'm using two S34ML08G1 NAND devices.

Labels (1)
Tags (2)
0 Kudos
1 Reply

662 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

one can check below link (attachments were sent via mail)

Adding Support For a New NAND with i.MX28–NAND Analysis 

On i.MX28 EVK with K9LBG08U0D there were 2-3MB/s results.

https://community.nxp.com/message/311702#311702 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos