We according to FRWY- LS1012A SDK (version 18.12) in the path of docs\lsdk_build_install.txt document line 85 description command download failed, wget is http://www.nxp.com/lgfiles/sdk/lsdk1812/firmware_ls1012afrwy_uboot_sdboot.img unbantu log is as follows:
root@vchip-virtual-machine:/home/work/flexbuild_lsdk1812# wget http://www.nxp.com/lgfiles/sdk/lsdk1812/firmware_ls1012afrwy_uboot_sdboot.img
--2019-03-06 03:27:03-- http://www.nxp.com/lgfiles/sdk/lsdk1812/firmware_ls1012afrwy_uboot_sdboot.img
Resolving www.nxp.com (www.nxp.com)... 23.205.248.208
Connecting to www.nxp.com (www.nxp.com)|23.205.248.208|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2019-03-06 03:27:04 ERROR 404: Not Found.
Hello liu xin,
I checked LSDK 1812 u-boot source code, for LS1012AFRWY platform, there is no SD u-boot at all, please refer to the following.
~/flexbuild_lsdk1812/packages/firmware/u-boot$ ls configs/ | grep ls1012afrwy
ls1012afrwy_qspi_defconfig
ls1012afrwy_qspi_SECURE_BOOT_defconfig
ls1012afrwy_tfa_defconfig
ls1012afrwy_tfa_SECURE_BOOT_defconfig
You could download QSPI u-boot image with the following command.
wget https://www.nxp.com/lgfiles/sdk/lsdk1812/firmware_ls1012afrwy_uboot_qspiboot.img
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------