使用MCUXpresso Config Tools v5配置MKE06Z128VLD4(LQFP44封装)引脚时,将pin11(PTI4)配置成IRQ,同时配置pin43为nRESET时,提示“配置有误”!为什么?是V5的BUG吗?还是不应该这样配置?谢谢!
另外,对pin11(PTI4)进行任何输入或输出配置时,代码预览均会消失,为什么?谢谢!
楼主你好,给我贴点问题图片看看。
另外,其实我个人认为,这么简单的引脚配置,完全可以直接从代码里面去配,很简单的。
直接修改寄存器SIM_PINSEL0[IRQPS]
没必要去用工具生成了。
Wish it helps you!
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------