Hello, my next hardware design will be in a high vibration environment in which case a crystal oscillator would not be a good fit. Instead, I would like to use a Mems oscillator. Is there any application notes, reference material, or comments on using a Mems clock instead of a crystal?
Thank you,
Joe
Solved! Go to Solution.
Have a great day,
I believe that there is not application note on using a Mems clock for the LS1012A. All four LS1012A reference boards I have checked use crystal. For sure you can use any clock oscillator which generates 25MHz single-ended square wave and satisfies Input DC and AC specifications for external clock oscillator/generator in the LS1012A datasheet. So I think it is better to ask Mems based oscillator producers if there is suitable one.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Have a great day,
I believe that there is not application note on using a Mems clock for the LS1012A. All four LS1012A reference boards I have checked use crystal. For sure you can use any clock oscillator which generates 25MHz single-ended square wave and satisfies Input DC and AC specifications for external clock oscillator/generator in the LS1012A datasheet. So I think it is better to ask Mems based oscillator producers if there is suitable one.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------